Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
cellular-slide9

Digi was able to work with Monster Media to illustrate the opportunity to utilize cellular and its benefits and equipped every station with a Digi Transport® WR21 Cellular Router connected via a Verizon 3G cell network. From their network operation center, Monster Media runs a Digi VPN concentrator to all of their displays to ensure a secure connection out to their assets.The cellular connection enables Monster Media to update content on the display—like relevant advertisements and games—to customize the experience for end-users. Monster Media’s robust Network Operating Center (NOC) uses Digi Device CloudSM to complement its capabilities. With the Digi TransPort WR21 and Device Cloud in place, Monster Media can collect data to determine the success of content. They can also monitor the health of platforms around the world. They know what systems are up and running properly, and which need rebooted or maintenance at any point in time. They can also send updates remotely.

PTM פורסם ב: