Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Product List
Image of EDATEC CM4 Industrial - Design Solution

CM4 industrial is an industrial embedded computer based on Raspberry Pi Compute Module 4, designed for IoT and industrial control data acquisition applications. It’s a reliable product, withstanding harsh working conditions such as extreme temperature ranges in the industrial environment. It has excellent heat dissipation performance due to its metal shell dissipating the heat of the CPU, wireless module, and power supply along with the heat-conducting silicone sheet, thereby dissipating heat from the device. It also features ESD protection to prevent surge and static electricity for interconnections. CM4 industrial has a support base and custom fixing screws on the PCB to prevent the PCB from being damaged due to force, and at the same time improve the reliability of the connection between the CM4 module and the PCB through screw fixing. It is also designed for standard DIN-rail mounts with flexibility for installation at the user’s site. It has various industrial communication interfaces and functions, such as RS232, RS485, high-precision analog-to-digital converter, and isolated I/O. It also has a Mini PCIe expansion interface which can be used to expand some peripheral modules, such as 4G, 5G, and NPU.

PTM פורסם ב: