Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List Associated Content
Quantum Architectural Advantage for Trion® Family

When compared to other competitive mid-range solutions, Efinix surpasses performance and utilization indices, while delivering industry leading power numbers. These are important features that are a determining factor for the success or failure of a system design using anyone's FPGAs. The XLR Logic element in the Quantum technology gives flexibility and scalability, allowing better utilization and lowering the complexity of the design. Due to this feature, the customer can accomplish the requirements more easily, at better power. In other architectures, the customer may need to move to the next device family member when utilization may only be 60-70%. With the Quantum architecture, the customer actually can utilize the amount of logic defined for that family member. Another benefit for the Quantum Architecture, is that it can be ported to other platforms very quickly and easily.

PTM פורסם ב: