Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
characteristics-slide7

eGaN® FET technology does not use an insulator in the gate. For this reason, the gate leakage current is higher than that of silicon MOSFETs. As can be seen in this slide, designers should expect gate leakage on the order of a few mA at 5V. As these devices have low gate-drive voltage, losses associated with gate leakage are low and therefore this is not an issue in most applications.

PTM פורסם ב: