Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
crystals-slide7

The cut angle of the crystal determines the vibration mode. “Flexural” mode with X cut has side-to-side oscillations enabling this tuning-fork shaped crystal unit to cover frequencies in the kHz band, such as 32.768kHz, which is commonly used as a clock frequency. “Thickness shear” mode with AT-cut has the top and bottom surfaces of the crystal chip move in opposite directions enabling it to cover frequencies ranging up to several hundred MHz. The stability vs. temperature curve of both modes can be characterized by the respective equations above.

PTM פורסם ב: