Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Product List
device enum2
The Interface descriptor is a related set of endpoints that present a single feature or function of the device to the host. It basically groups endpoints into a functional group performing a single feature of the device. Endpoint descriptors describe endpoints other than endpoint zero. Endpoint zero is always assumed to be a control endpoint and is configured before any descriptors are even requested. (The Endpoint is memory buffer allocated on the device for sourcing or sinking the data on the USB bus). Finally are the optional String descriptors, which provide human readable information.
PTM פורסם ב: