Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Product List
usb elec2
A USB device can be either powered by the upstream Host or Hub port, or have its own power supply. If the device is powered by the upstream port, it is considered Bus-powered and can draw no more than 100mA before it is enumerated. After enumeration, it can be configured to draw up to 500mA. The USB specification includes mechanisms for sensing over-current conditions and shutting down a device in an over-current state. If a device has its own power supply, which is common not only for devices that require more than 500mA but also for battery-powered devices, then it is considered self-powered.
PTM פורסם ב: