Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Product List
tools4
Vinculum Customizer is a handy tool to customize some of the standard features of VNC1L firmware, such as command modes, UART options, firmware options, USB slave mode settings, code page selection, and version code. VPLAY is used in conjunction with the VMUSIC2 module and a TTL232R cable to provide a GUI for playing audio files. VPROG is the VNC1L programming utility that downloads firmware onto a VNC1L device using the FTDI TTL-232R-3V3 cable. A COM port version is also available.
PTM פורסם ב: