Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Product List
vinc3
VDPS (Vinculum Disk, PC monitor and Slave port) firmware is used if a microcontroller needs both USB Host functionality and will connect to a host port on a PC. The VNC1L will enumerate as an FTDI FT232 device and cause the PC to load the same FTDI VCP and/or D2XX device drivers used for the FTDI device chips.  Data from the PC is then transferred to the VNC1L monitor port. The PC USB Host port can only be connected through the VNC1L Port 1.
PTM פורסם ב: