Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Product List
usb architecture1
The USB architecture is a tiered architecture where the USB Host controller controls all the USB bus activities. Up to 127 USB Devices can be connected in a daisy chain format using logical devices like USB hubs, but can not exceed 7 tiers. The host is responsible for device detection (attachment-detachment), dynamically loading the driver (enumeration), dynamically unloading the drivers on device removal, power allocation (bus powered, self powered), and protection against overdrawn current events. The blocks in the drawing marked “Func” in the tiered architecture figure stand for “Functional device”, such as a USB mouse, keyboard, flash drive, etc. One may connect the functional devices through a logical device like a USB hub.
PTM פורסם ב: