Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Product List
usb architecture2
Logical devices perform logical fan out with the capability of synchronizing different data rate operations. For example, a USB hub may act as a bridge between a high speed Host and a low speed device. The hub is a logical translator between two operational speeds. If a second high speed device connects to the same hub, then the hub will allow high speed data transfer while maintaining the low speed connection to the low speed device. “Compound” devices implement two or more logical devices within a single functional device. For example, a keyboard may have an integrated USB hub for supporting flash drive or mouse.
PTM פורסם ב: