Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Product List
ftdi device2 FTDI Drivers website
Since FTDI devices enumerate as a custom class, they need specific drivers to be installed on the PC. In conjunction with the USB device ICs, FTDI provides a complete, royalty-free solution of device drivers at the application and bus layers. An RS232 serial port application can be used without modification and by just using the VCP driver. The VCP driver causes the USB device to appear as an additional COM port available to the PC. Application software can access the USB device in the same way as it would access a standard COM port. The VCP driver is used in conjunction with the FTDI D2XX bus driver.
PTM פורסם ב: