Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Product List
what is usb2
USB evolved as the universal serial bus that can handle multiple devices (up to 127), loads device drivers automatically (standard USB drivers), has configurable operational details, can detect power configuration, and can determine the speed of operation. Most importantly, it detects the device state. If the device is unplugged from the system, it dynamically unloads the drivers to save system resources. All of these USB transactions are controlled through a single USB Host (master) that is responsible for all of the USB device (client or slave) support. The host provides power and loads the device drivers needed during enumeration, thus enabling a plug-and-play experience to end users. The devices are also known as “functional” devices in USB specifications, as they perform a specific functional class of operation like Mass Storage Device (MSD), Human Interface Device (HID), and Communications Device Class (CDC). Compound devices are formed when two different classes are operated on the same device. An HID device such as a keyboard, which also supports a flash drive interface (MSD), is a classic example of a compound device.
PTM פורסם ב: