Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Product List
vinc5
VDFC (Vinculum Disk and File Copier) firmware allows VNC1L to connect two BOMS devices on Port1 and Port2, then carry out disk and file copy operations between the disks. Port1 is always the source disk and Port2 is always the target in this firmware. The Monitor port and GPIO pins are used to carry out disc and file copy commands.
PTM פורסם ב: