Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
Benefits of Radar Technology

For many years, radar devices had to deal with the prejudice of being “too complex and too expensive". Now, however, more and more radar-based products conquer the market due to their benefits. Radar is an anonymous and touchless measurement technology. It works for both indoor and outdoor applications because the performance of the detection is not affected by weather conditions like rain, snow, or fog. It also works in the dark and in challenging light conditions. Radar devices can also be used in harsh environments; dust, vibration, noise, heat, and cold do not influence the object measurement. Radar waves are able to radiate through a wide range of materials, so it can be hidden in places such as behind a plastic covering. It detects objects, people, or vehicles in far distances, and vandalism actions like graffiti or bubble gum in front of the antenna do not impair the detection. This makes radar one of the most reliable and robust measurement technologies available.

PTM פורסם ב: