Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List
KO-CAP®

Along with MLCC and in order to avoid aging and DC bias, a designer must consider using KEMET’s polymer capacitor KO-CAPs®. A typical construction detail of a KO-CAP is shown here. Tantalum polymer capacitors have a tantalum pentoxide dielectric with a polymer cathode. This polymer material can actually consume oxygen and makes it nonconductive, which is what differentiates polymer from the traditional tantalum capacitors. Since most applications do require long-term reliability, KEMET recommends that designers consider a voltage derating, as shown in the graph here, for the maximum steady state voltage. The biggest advantage of this capacitor technology is the ability to pack a lot of storage into a small package. While the ESR might not be as low as an MLCC, it still has a low ESR. These devices are mostly used in under 1 MHz frequency range without self resonance effects.

PTM פורסם ב: