Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
Human Detection by Pyroelectric Effect

The top chart on this slide shows the different types of electromagnetic waves found in the air. The focus is on the infrared ray between 780 nm to 1 mm. In the infrared ray only, a specific portion is the area of the pyroelectric infrared sensor detection as seen here. The major application is for human detection.

PTM פורסם ב: