Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
Introduction to Microphones Slide 4

The image on this slide is an example of a microphone frequency response curve. It shows the voltage in dB relative to 1 Vrms, for a sound pressure of 0.1 Pascal. The voltage output at 1 kHz is referred to as the sensitivity. Both reference sound pressures (1 Pascal and 0.1 Pascal) are in common usage; 1 Pascal sensitivity is 20 dB greater than 0.1 Pascal sensitivity.

PTM פורסם ב: