Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Product List
LT3756-Slide7

The LT3756-2's demoboard is the DC1319B-A. This is a single sided PC board with all of the components mounted on the top side. The LT3756-2’s entire solution footprint can be fit into only 25mm x 30mm. If a double layer PC board were used and components were mounted on both sides of the board, the area of solution footprint could be reduced by 50%. All of the components used in this design are low profile enabling a very compact over all solution.

PTM פורסם ב: