Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
Ethernet-Slide15

This schematic figure shows the recommended solution for intra-building exposed 10BaseT and 100BaseT systems. This is a solution for non PoE systems only. The SP03-3.3 is a grounded TVS diode array. It is very robust with a 150A, 8x20 surge current rating which is currently 50% higher than other available offerings on the market. A TeleLink® fuse provides the power cross overcurrent protection which is needed by some customers. While only one fuse is shown per data pair, engineers will find that putting a fuse in each line improves the line balance.  Some designs have been granted a waiver that allows them to do without the fuses.

PTM פורסם ב: