Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Product List
Image of Lumissil CS897x Line of 8-bit Microcontrollers - Software

Lumissil’s development kit also comes with software and documentation to build an application. The code is written in the Microsoft Visual Studio Code Environment. In here the customer will manage the project, write and edit the code, compile and debug the program, and it is free to use. Also, Lumissil provides a large selection of example code and in-depth user guides.

PTM פורסם ב: