Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
AODAK-Slide9

The Reference Design 24 board is the heart of the kit. This analog output module includes all of the signal chain components for a flexible and scalable multi-channel design. This sub-system consists of three interfaces: a slave SPI interface which terminates with the master SPI port of a microcontroller, a power supply input, and the analog output interface which in a complete system would connect to a passive I/O board with circuit protection diodes.

PTM פורסם ב: