Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
CLC-Slide6

Some examples of applications of the CLC are implementation of synchronous gates, power sequencing, and Manchester encoding. A pair of CLCs may be combined to implement more complex logic functions, such as a data modulator. The example shown on this slide is a Phase Shifted Data modulator using the CLC module. As shown in this example the output of one CLC module may be used as an input to another CLC module.

PTM פורסם ב: