Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
LDO-Slide7

The MCP172x LDOs are the most feature-rich in the family and include a power good output and  power good delay functions. The power good output can be used to signal when the output is within 92% of nominal regulation value, while the power good delay can change the timing of this signal between 200μs and 300ms for a improved power management.

PTM פורסם ב: