Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
MCP20-Slide10

The new MCP2050, MCP202XA and the MCP2003A all meet the 2011 requirements listed on this slide. The ESD on the two new parts exceed 15kV (IEC-61000-2) which shows the part robustness within tough environmental conditions. The portfolio also has some of the lowest current on the market with typical powerdown current ratings at less than 4.5µA. The enhanced voltage regulator comes in both 3.3V or 5.0V options with 70mA output. The current limit of 250mA allows for higher than 70mA to be supported when thermal characteristics are taken in to consideration such as heat dissipation.

PTM פורסם ב: