Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
MCP3901-Slide7

As mentioned previously, the MCP3901 boasts a lower power consumption of only 14mW at 5V. The MCP3901 also has an adjustable sample rate up to 64ksps. In order to maintain low power, this high frequency sample rate uses a special current boost mode so that lower sample frequencies do not operate with the same current consumption.

PTM פורסם ב: