Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
Low-Slide11

The data transfer rate for DDR memory is always increasing and will continue to increase as the need for higher data transfer speeds and huge data processing requirements increase. As a result of the transfer rate increase, the frequency and magnitude of the ripple voltage also increases. In order to solve the ripple voltage problem, Low ESL capacitors are recommended as a solution to bypass the high speed noise and also conserve board space.

PTM פורסם ב: