Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List
NX3Lxxx 2
The next four digits indicate the function type. If the devices integrates a special function, such as shunt resistors, negative swing or an enable pin, it will be indicated in this section. Finally, the last two letters indicate the package type. So an NX3L1G3157GW is a Single SPDT analog switch with 3 volt VCC capability, 1 ohm or lower RON, in an SOT886 package.
PTM פורסם ב: