Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Product List
theory2
As shown on this slide, if the Input pin is driven HIGH, the output of inverter A is set low. This low level turns off the NMOS device and turns on the PMOS device, pulling the input high. If the driver is removed, the CMOS input buffer remains defined as a logic high.
PTM פורסם ב: