Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Product List
3 op modes

The LPC3250 can operate in three modes. If the device is in RUN mode, it indicates that the application needs the CPU, AHB bus, or one of the peripherals that runs faster than SYSCLK. In this mode, the CPU will run typically at 266 MHz and the AHB bus would run at 133 MHz. In the DIRECT RUN mode, the running application does not need the CPU, the AHB bus, and the peripherals to run faster than SYSCLK. This is the default mode after chip reset.

PTM פורסם ב: