Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Product List
usb block
The USB block can be used either as a device, host, or in an OTG configuration. It supports all four transfer types, does not support high speed, and has its own dedicated DMA controller. Additionally, there are two SPI and two SSP controllers. The SPI controllers can only be used in Master mode with bit rates up to 52Mbits/sec while the SSP controller has eight frame FIFOs for both Tx and Rx. Each frame can accommodate between 4 to 16 bits.
PTM פורסם ב: