Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Product List
10 100 eth mac
Ethernet MAC is also supported and it interfaces to the external PHY using the MII or RMII protocol. Typically, the MDC frequency should not be more than 2.5MHz. In the LPC3250 implementation, the minimum attainable MDC frequency will be 3.714MHz. To avoid this issue, either limit the HCLK to 52MHz or select an Ethernet PHY that supports MDC frequencies above 3.714MHz. This behavior will most likely not be noticed since most external PHYs support higher frequencies.
PTM פורסם ב: