Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Product List
interrupt control
The interrupt controller is made up of three blocks – the Main Interrupt Controller (MIC), the Sub1 Interrupt Controller (SIC1), and the Sub 2 Interrupt Controller (SIC2). The output of the interrupt controller drives IRQ and FIQ to the main CPU. Interrupt priority is fixed and is in direct correspondence to the way the peripherals are connected to the controller. As an example, the Ethernet interrupt is connected to the MIC whereas the USB interrupts are connected to the SIC1. When an interrupt occurs, the application has to go through the MIC, SIC1, and/or SIC2 status registers and search for the source of the interrupt. Also, as a note, the interrupt controller does not operate in STOP mode. The start sources connected to the START controller will help the device to exit STOP mode.
PTM פורסם ב: