Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Product List
on reset
On reset, the device will come up in Direct RUN mode. From here, the device can switch to either STOP or RUN mode. Assume the device wants to switch to RUN mode. This can be achieved in software by writing 1 to bit 2 of the power control register. By resetting this bit, the device will reenter Direct Run mode. The device enters STOP mode by setting bit 0 of the same register. Wakeup from STOP mode is configured in the start controller. It is not possible to switch directly from STOP to RUN mode, and vice versa.
PTM פורסם ב: