Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Product List
touch screen control
The LPC32x0 includes a touch screen controller (TSC) that can operate in two different modes. In AUTO mode, the touch screen will automatically collect the X and Y coordinates of the pressed position. In MANUAL mode the controller can be sequenced entirely by software to collect the coordinates of the pressed position. This controller also operates as a three channel, 10-bit successive ADC. The analog portion of the ADC has its own power supply to enhance the low noise characteristics of the converter. A total of 87 pins can potentially be used as general purpose input/outputs (IOs). Also, an automatic keyboard scanner function is also provided that supports 8 x 8 keys. The 8-channel, general purpose DMA controller supports several peripherals including the SD card, the high speed UARTs, the I2S ports, and the SPI interfaces. Also, as mentioned earlier, dedicated DMA controllers are available for the USB, the Ethernet and the LCD controller.
PTM פורסם ב: