Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Product List
etm9
The ETM provides a real-time trace capability for deeply embedded processor cores. It outputs information about processor execution to the ETB. Also, a software debugger that allows configuration of the ETM using a JTAG interface is able to display the trace information that has been captured, in a format that a user can easily understand. The ETB stores trace data produced by the ETM in a 2K trace RAM that is used for instruction and data history storage. Tools like ARM RealView ICE and the RealView debugger will support this feature.
PTM פורסם ב: