Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Product List
power domain switch
The RTC clock is on a separate power domain and has 32 words of low-power SRAM. To save the maximum amount of power, the microcontroller power can be turned off altogether while keeping the RTC alive with some critical system information that can be saved between power cycles. This also eliminates leakage current power consumption. Each peripheral and the AHB matrix has a selectable Clock Enable bit. Therefore, the application can control which combinations of peripherals to enable for its particular system design and also when to enable them. Further, several peripherals have local power saving modes (such as sleep modes) available for more power savings. Additionally, the AHB clock can be divided to run at a lower frequency so that the entire matrix can run at a lower frequency.
PTM פורסם ב: