Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
SA604AD
The SA604AD and SA614AD are an FM IF subsystem; meaning that it has no internal down mixer. It contains the IF and limiter amplifiers, Received Signal Strength Indicator (RSSI) and quadrature detector and the Muted and Unmuted Audio outputs. The SA604AD and SA614AD are used with the SA602AD mixer to provide a single conversion receiver.
PTM פורסם ב: