Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
Slide15

MOSFET relays can easily replace photocouplers and MOSFET chips saving space and adding cost savings as well. MOSFET relays can also replace electromechanical relays; not only 1 form A, but also 1 form C relays, with the addition of a NAND gate to create a SPDT contact. The NAND gate swaps Vcc between the two control inputs of the FET to create a NC and NO contact. The amount of energy required is fractional as compared to a mechanical relay.

PTM פורסם ב: