Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
sig bounce
Signal bounce also needs to be considered when utilizing detector switches. When the internal spring touches the contact, there is signal chatter. This is completely normal but needs to be corrected via a microprocessor. The engineer recommends the microprocessor to read three times or more at 3 ms. Also, the engineer recommends an RC circuit integration with time constant of 6 ms or more.
PTM פורסם ב: