Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Product List Associated Content
ASCII Software Command Set

The PAN9420 contains over 100 ASCII software commands to configure and control the module. Example WLAN commands shown here are “get wlan ssid sta” to read the modules SSID name, in this case Interdimensionial Wifi. “Get wlan ssid ap” to read its access point name, in this case PAN9420_AP. Other examples include “get wlan state sta” to return whether the module is off or on and “get wlan status sta” to return one of ten values showing the modules current status.

PTM פורסם ב: