Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
in off mode
The LinkZero-AX device will still provide power in the off-mode. Even while main switching is disabled, the bypass pin provides a regulated 4 V output that can source up to 500 µA. This provides a constant local auxiliary supply that can be used to power systems when the main appliance is in standby. For example, this supply could be used to power a motion sensor in a security system or an infrared remote control sensor for a TV. During normal operation, some of the bypass pin power is used to operate the LinkZero-AX device itself, so the bypass pin can only provide 85 µA. If more power is needed, it can be supplied from the output rail or through a separate bias winding on the transformer.
PTM פורסם ב: