Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
Thermal Resistance for Thermal Conduction

This diagram illustrates how heat at temperature T1 at one end of an object (looking at cross-sectional area A and length L) reaches the other end at temperature T2 by conduction. When the cross-sectional area of the object is increased or the length is shortened, the thermal resistance of the conductor decreases. The equation to determine (T1 - T2) consequently becomes the thermal resistance (Rth) times the heat flow (P), in keeping with the “Thermal Ohm’s Law”. To decrease the thermal resistance: increase the cross section of the object, decrease the length of the object, or select material with a higher thermal conductivity.

PTM פורסם ב: