Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List Associated Content
performance lvds

On this slide, the graph shows the results of maximum transient frequency deviation in response to mechanical shock tests on selected differential oscillators. The competitor 1 and competitor 2 devices are SAW based and are especially sensitive to shock, with over 10 ppm of transient frequency spike. Other quartz devices exhibited 2 to 4 ppm of peak frequency deviation. The only exception is the SiTime device, which demonstrated a transient frequency deviation of <1 ppm.

PTM פורסם ב: