Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
Power-Slide11

This slide shows the salient features of a micro-power MHz oscillator which can be leveraged for a wearable design. First, its size with the smallest footprint of 1.2mm².  Second, its low power with a core current draw of only 60µA. This is 18% lower than the current consumption of a MHz oscillator circuit on a leading ultra-low-power MCU.

PTM פורסם ב: