Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Product List
Smart Grid Solutions: Smart Grid Distribution/Smart Meters Slide 12

Shown on this slide is a simplified block diagram of a typical Smart Meter. As can be seen, the main function of the basic E-meter is the functionality, which measures the energy. Microcontrollers with dlms (device language message specification) protocols work with the data. The system also includes a power supply for the meter, embedded security, memory for the data, a reliable real-time clock, and anti-tamper protection with ST’s sensor devices. The information is transferred either through the power line, inside the house through the network with RF transceivers, or via the power line modem.

PTM פורסם ב: