Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Product List
Smart Grid Solutions: Smart Grid Distribution/Smart Meters Slide 26

A snapshot on the power line communication roadmap is presented on this slide, beginning with a protocol independent, narrowband transceiver which was developed a long time ago and is still sold in the market as the ST7538 and ST7540. The next platform is called STarGRID, which is evolving in protocols in the Prime Alliance, Iberdrola, and the Enel/Endesa. It is more of an integrated SOC solution for multiple standard narrowband PLCs which allows approaching the home market at different speeds with different systems and the different needs.

PTM פורסם ב: