Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Product List
Smart Grid Solutions: Smart Grid Distribution/Smart Meters Slide 20

ST has developed a dedicated transceiver which is called SPIRIT1. This is a sub 1-GHz unit which is actually not any taller than a 100 MHz transceiver, but it ranges, with proper adaptation on the antenna and the transmission network, from 169 MHz to 956 MHz which is all of the allowed bandwidth in Europe, the United States, and Asia. The user can decide which one is best for their use and work with it. Several modulation schemes are available for the SPIRIT1 from FSK to GFSK, MSK, OOK, and ASK. Plus it offers high data rates, up to 500 kbps. Some of the most important features of this device are the sensitivity and low power consumption. The programmable output power ranges from -30 dBm to +12 dBm power, and the programmable channel spacing, 12.5 kHz minimum, is narrow to allow working with more channels. Frequency hopping is also allowed if needed in an application. AES 128-bit encryption is embedded. Additionally, antenna diversity is featured enabling the user to embed different antennas. ST has developed an embedded MAC on the chip, because it is more than a standard transceiver. It supports several standards, particularly the wireless M-BUS and the 6LowPan, plus a basic stack and a simple stack from ST that enables the user’s simple network implementation as well.

PTM פורסם ב: