Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Product List
Smart Grid Solutions: Smart Grid Distribution/Smart Meters Slide 18

Shown on this slide is the evaluation board for the STM32W. The STM32W108xx kits provide demonstration applications and documentation which serve as a reference for creating applications and re-programming the STM32W108xx microcontroller. The user can run the STM32W108xx kits in several ways (remote control/target, HID devices such as a mouse or keyboard, and point-to-point applications), using the dedicated software libraries (ZigBee RF4CE, and Simplified MAC), as well as a third-party IDE and C compiler (IAR). Also included is a complete feature set with GUI, application notes, data sheets and anything needed to develop an application.

PTM פורסם ב: