Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Product List
Smart Grid Solutions: Smart Grid Distribution/Smart Meters Slide 22

There is a development kit available for the SPIRIT1 module which consists of two main boards. The development kit comes with a daughter board which includes the SPIRIT1 chipset, plus a mother board with an STM32L onboard, and ST provides libraries and stack in order to evaluate the communication. The kit also includes a graphical user interface and two antennas for communication. The daughter board has an SMA connector enabling the user to attach the proper antenna for the application. With this kit the user can perform the performance test and any other tests needed to make the pre-development using the ST devices.

PTM פורסם ב: